REGEN.TEMPWTHRESH

Description

This parameter returns the over temperature warning threshold of the power circuit for the regen resistor. The value depends on the drive model. It is programmed in the drive and cannot be changed.

Versions

Action

Version

Notes

Implemented

02-08-01-000

General Information

Type

Read Only

Units

Deg C

Range

N/A

Default Value

N/A

Data Type

Float

See Also

 

Stored in Non-Volatile Memory

 

Variants Supported

All variants are supported.

Industrial Ethernet Information

(missing or bad snippet)